public interface MoveNode extends ProgramNode
| Modifier and Type | Method and Description |
|---|---|
MoveNodeConfig |
getConfig() |
MoveNodeConfigFactory |
getConfigFactory() |
MoveNode |
setConfig(MoveNodeConfig config)
Set a configuration on this node.
|
MoveNodeConfigFactory getConfigFactory()
MoveNode setConfig(MoveNodeConfig config)
config - the configuration to be set.IllegalArgumentException - if this node is a MoveP containing one or more CircleMoveNode and the node configuration is attempted to be changed to MoveJ or MoveL.
CircleMoveNode is only allowed under a MoveP. All instances of CircleMoveNode need to be deleted before the configuration can be changed from a MoveP to MoveJ or MoveL.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)MoveNodeConfig getConfig()
Copyright © 2018. All rights reserved.