public interface IfNode extends ProgramNode
| Modifier and Type | Method and Description |
|---|---|
String |
getExpression()
Deprecated.
Use
getExpression2() instead |
Expression |
getExpression2() |
IfNode |
setExpression(Expression expression) |
IfNode |
setExpression(String expression)
Deprecated.
Use
ExpressionBuilder to build an
Expression and set it using setExpression(Expression expression) |
@Deprecated IfNode setExpression(String expression)
ExpressionBuilder to build an
Expression and set it using setExpression(Expression expression)expression - The expression that will be evaluated in this IfNodeIllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)IfNode setExpression(Expression expression)
expression - The expression that will be evaluated in this IfNodeIllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)@Deprecated String getExpression()
getExpression2() insteadExpression getExpression2()
Copyright © 2018. All rights reserved.