public interface ElseIfNode extends ProgramNode
| Modifier and Type | Method and Description |
|---|---|
String |
getExpression()
Deprecated.
Use
getExpression2() instead |
Expression |
getExpression2() |
ElseIfNode |
setExpression(Expression expression) |
ElseIfNode |
setExpression(String expression)
Deprecated.
Use
ExpressionBuilder to build an
Expression and set it using setExpression(Expression expression) |
@Deprecated ElseIfNode setExpression(String expression)
ExpressionBuilder to build an
Expression and set it using setExpression(Expression expression)expression - The expression that will be evaluated in this ElseIfNodeIllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)ElseIfNode setExpression(Expression expression)
expression - The expression that will be evaluated in this ElseIfNodeIllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)@Deprecated String getExpression()
getExpression2() insteadExpression getExpression2()
Copyright © 2018. All rights reserved.