public static enum IO.InterfaceType extends Enum<IO.InterfaceType>
Enum Constant and Description |
---|
UR_CONFIGURABLE |
UR_EUROMAP |
UR_GENERAL_PURPOSE |
UR_MODBUS |
UR_STANDARD |
UR_TOOL |
Modifier and Type | Method and Description |
---|---|
static IO.InterfaceType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static IO.InterfaceType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final IO.InterfaceType UR_STANDARD
public static final IO.InterfaceType UR_TOOL
public static final IO.InterfaceType UR_CONFIGURABLE
public static final IO.InterfaceType UR_MODBUS
public static final IO.InterfaceType UR_GENERAL_PURPOSE
public static final IO.InterfaceType UR_EUROMAP
public static IO.InterfaceType[] values()
for (IO.InterfaceType c : IO.InterfaceType.values()) System.out.println(c);
public static IO.InterfaceType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2018. All rights reserved.