| Interface | Description |
|---|---|
| ContributionProvider<C> |
This interfaces provides access to a contribution.
|
| DaemonContribution |
Defines an API definition that gives control of a daemon that belongs to a URCap.
|
| DaemonService |
Defines an API that makes it possible to define daemons of a URCap within PolyScope.
|
| InstallationNodeContribution |
API for installation node contributions.
|
| InstallationNodeService |
Defines an API required for definition of an installation node and screen of a URCap.
|
| NonUserInsertable |
This interface is a marker interface that can be used in combination with
ProgramNodeService. |
| ProgramNodeConfiguration |
Provides access to configure additional properties of a program node contribution with a HTML-based user interface.
|
| ProgramNodeContribution |
Defines an API required for specifying a URCap Program Node within PolyScope.
|
| ProgramNodeService |
Defines an API required for adding a new type of program node to PolyScope.
|
| ProgramNodeServiceConfigurable |
This interface can be used in combination with the
ProgramNodeService interface. |
| URCapProgramNodeService | |
| ViewAPIProvider |
Provides access to functionality relevant for the View (UI) of an installation or a program node
contribution.
|
| Enum | Description |
|---|---|
| DaemonContribution.State |
RUNNING - The daemon is running
STOPPED - The daemon is stopped
ERROR - The daemon should be running but it is not
|
Copyright © 2018. All rights reserved.