public static enum SelectEvent.EventType extends Enum<SelectEvent.EventType>
ON_SELECT - an event of this type is issued when an element is selected. For example when the user selects an item in a drop-down list.
Enum Constant and Description |
---|
ON_SELECT |
Modifier and Type | Method and Description |
---|---|
static SelectEvent.EventType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static SelectEvent.EventType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final SelectEvent.EventType ON_SELECT
public static SelectEvent.EventType[] values()
for (SelectEvent.EventType c : SelectEvent.EventType.values()) System.out.println(c);
public static SelectEvent.EventType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2018. All rights reserved.