public static enum Pressure.Unit extends Enum<Pressure.Unit>
| Enum Constant and Description |
|---|
ATM
Standard atmosphere [atm].
|
BAR
Metric unit of pressure [bar].
|
INHG
Inch of mercury at 32°F [inHg] imperial unit.
|
KPA
Kilo newton per square metre [kPa].
|
MBAR
Metric unit of pressure [mbar].
|
PA
Newton per square metre (Pascal) [Pa] SI unit.
|
PSI
Pounds per square inch [lbf/in²] imperial unit.
|
| Modifier and Type | Method and Description |
|---|---|
static Pressure.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Pressure.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Pressure.Unit PA
public static final Pressure.Unit KPA
public static final Pressure.Unit MBAR
public static final Pressure.Unit BAR
public static final Pressure.Unit ATM
public static final Pressure.Unit PSI
public static final Pressure.Unit INHG
public static Pressure.Unit[] values()
for (Pressure.Unit c : Pressure.Unit.values()) System.out.println(c);
public static Pressure.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2021. All rights reserved.