public static enum Mass.Unit extends Enum<Mass.Unit>
| Enum Constant and Description |
|---|
KG
Kilograms [kg] SI unit.
|
LB
Pounds [lb] imperial unit.
|
| Modifier and Type | Method and Description |
|---|---|
static Mass.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Mass.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Mass.Unit KG
public static final Mass.Unit LB
public static Mass.Unit[] values()
for (Mass.Unit c : Mass.Unit.values()) System.out.println(c);
public static Mass.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2021. All rights reserved.