public static enum AngularAcceleration.Unit extends Enum<AngularAcceleration.Unit>
| Enum Constant and Description |
|---|
DEG_S2
Degrees per second squared [°/s²].
|
RAD_S2
Radians per second squared [rad/s²] SI unit.
|
| Modifier and Type | Method and Description |
|---|---|
static AngularAcceleration.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AngularAcceleration.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final AngularAcceleration.Unit RAD_S2
public static final AngularAcceleration.Unit DEG_S2
public static AngularAcceleration.Unit[] values()
for (AngularAcceleration.Unit c : AngularAcceleration.Unit.values()) System.out.println(c);
public static AngularAcceleration.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2021. All rights reserved.