| AnalogInputUntilNodeConfig |
| AnalogInputUntilNodeConfig.InputDomainType
The type of the electrical domain used by an analog input.
|
| BlendParameters |
| BlendParameters.ParameterType
Blend Parameters can be of different types
The parameter type is used to determine the explicit blend parameters (can be used in place of instanceof operations).
|
| CustomDecelerationParameters |
| CustomDecelerationParameters.Type |
| DecelerationParameters |
| DecelerationParameters.ParameterType
The deceleration parameter type used to determine which type of deceleration parameter this instance is.
|
| DigitalInputUntilNodeConfig |
| DistanceUntilNodeConfig |
| ExpressionUntilNodeConfig |
| FloatRegisterInputUntilNodeConfig |
| IOInputUntilNodeConfig |
| IOInputUntilNodeConfig.SelectionType
The type of the input selection.
|
| ReachedWaypointUntilNodeConfig |
| UntilNodeConfig
This interface represents a configuration of the Until program node.
|
| UntilNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|