public interface UntilNodeConfigFactory
| Modifier and Type | Method and Description |
|---|---|
AnalogInputUntilNodeConfig |
createAnalogInputConfig(AnalogIO input,
CompareOperator compareOperator,
Current currentThreshold,
ErrorHandler<Current> errorHandler)
Creates an I/O Input configuration for an Until node.
|
AnalogInputUntilNodeConfig |
createAnalogInputConfig(AnalogIO input,
CompareOperator compareOperator,
Voltage voltageThreshold,
ErrorHandler<Voltage> errorHandler)
Creates an I/O Input configuration for an Until node.
|
BlendParameters |
createBlendParameters(Blend suggestedBlend)
Creates blend parameters for an Until node.
|
CustomDecelerationParameters |
createDecelerationParameters(Acceleration deceleration,
ErrorHandler<Acceleration> decelerationErrorHandler)
Creates deceleration parameter for an Until node.
|
CustomDecelerationParameters |
createDecelerationParameters(AngularAcceleration deceleration,
ErrorHandler<AngularAcceleration> decelerationErrorHandler)
Creates deceleration parameter for an Until node.
|
CustomDecelerationParameters |
createDecelerationParameters(AngularAcceleration angularDeceleration,
ErrorHandler<AngularAcceleration> angularDecelerationErrorHandler,
Acceleration cartesianDeceleration,
ErrorHandler<Acceleration> cartesianDecelerationErrorHandler)
Creates deceleration parameter for an Until node.
|
DigitalInputUntilNodeConfig |
createDigitalInputConfig(BooleanRegister input,
boolean valueToProceedUntil)
Creates an I/O Input configuration for an Until node.
|
DigitalInputUntilNodeConfig |
createDigitalInputConfig(DigitalIO input,
boolean valueToProceedUntil)
Creates an I/O Input configuration for an Until node.
|
DigitalInputUntilNodeConfig |
createDigitalInputConfig(ModbusIO input,
boolean valueToProceedUntil)
Creates an I/O Input configuration for an Until node.
|
DistanceUntilNodeConfig |
createDistanceConfig()
Creates a Distance configuration for an Until node with PolyScope default values.
|
DistanceUntilNodeConfig |
createDistanceConfig(Length distance,
ErrorHandler<Length> distanceErrorHandler,
BlendParameters blendParameters)
Creates a Distance configuration for an Until node.
|
ExpressionUntilNodeConfig |
createExpressionConfig()
Creates an Expression configuration for an Until node with PolyScope default values.
|
ExpressionUntilNodeConfig |
createExpressionConfig(Expression expression)
Creates an Expression configuration for an Until node with an expression and default value for the deceleration
parameter.
|
ExpressionUntilNodeConfig |
createExpressionConfig(Expression expression,
DecelerationParameters deceleration)
Creates an Expression configuration for an Until node.
|
FloatRegisterInputUntilNodeConfig |
createFloatRegisterInputConfig(FloatRegister input,
CompareOperator compareOperator,
float threshold)
Creates an I/O Input configuration for an Until node.
|
IOInputUntilNodeConfig |
createIOInputConfig()
Creates an I/O Input configuration for an Until node with PolyScope default values, i.e.
|
BlendParameters |
createNoBlendParameters()
Creates no blend parameters for an Until node.
|
ReachedWaypointUntilNodeConfig |
createReachedWaypointConfig()
Creates a Reached Waypoint configuration for an Until node.
|
DecelerationParameters |
createSharedDecelerationParameters()
Creates shared deceleration parameter for an Until node.
|
BlendParameters createNoBlendParameters()
Creates no blend parameters for an Until node. The robot arm will stop without performing a blend.
Can be used in a Distance configuration type.BlendParameters createBlendParameters(Blend suggestedBlend)
suggestedBlend - This blend value may be (automatically) corrected depending on the value of the
distance parameter the Distance configuration.DecelerationParameters createSharedDecelerationParameters()
Creates shared deceleration parameter for an Until node. The acceleration values from the parent Move node will be used as deceleration (absolute value).
Can be used in an Expression configuration type.CustomDecelerationParameters createDecelerationParameters(AngularAcceleration deceleration, ErrorHandler<AngularAcceleration> decelerationErrorHandler)
Creates deceleration parameter for an Until node. Can be used in an Expression configuration type.
An angular deceleration is used when the type of the parent Move node is a MoveJ, whereas a Cartesian deceleration is used when the move type is a MoveL or MoveP.deceleration - the angular deceleration (the value for the Cartesian deceleration will be the default value
that PolyScope uses), not null.decelerationErrorHandler - error handler for handling validation. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid angular deceleration value.CustomDecelerationParameters createDecelerationParameters(Acceleration deceleration, ErrorHandler<Acceleration> decelerationErrorHandler)
Creates deceleration parameter for an Until node. Can be used in an Expression configuration type.
An angular deceleration is used when the type of the parent Move node is a MoveJ, whereas a Cartesian deceleration is used when the move type is a MoveL or MoveP.deceleration - the Cartesian deceleration (the value for the angular deceleration will be the default value
that PolyScope uses), not null.decelerationErrorHandler - error handler for handling validation. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid cartesian deceleration value.CustomDecelerationParameters createDecelerationParameters(AngularAcceleration angularDeceleration, ErrorHandler<AngularAcceleration> angularDecelerationErrorHandler, Acceleration cartesianDeceleration, ErrorHandler<Acceleration> cartesianDecelerationErrorHandler)
Creates deceleration parameter for an Until node. Can be used in an Expression configuration type.
An angular deceleration is used when the type of the parent Move node is a MoveJ, whereas a Cartesian deceleration is used when the move type is a MoveL or MoveP.angularDeceleration - the angular deceleration, not null.angularDecelerationErrorHandler - error handler for handling validation. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid angular deceleration value.cartesianDeceleration - the Cartesian deceleration, not null.cartesianDecelerationErrorHandler - error handler for handling validation. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid cartesian deceleration value.ExpressionUntilNodeConfig createExpressionConfig()
Creates an Expression configuration for an Until node with PolyScope default values. This default configuration corresponds to when the end user inserts a new Until Expression node in the program tree manually.
Note that these default values may change between PolyScope versions.ExpressionUntilNodeConfig createExpressionConfig(Expression expression)
Creates an Expression configuration for an Until node with an expression and default value for the deceleration parameter. The until condition for this configuration is true once the evaluation of the expression is true.
Note that this default value may change between PolyScope versions.expression - the expression whose evaluation will determine whether the until condition is met.ExpressionUntilNodeConfig createExpressionConfig(Expression expression, DecelerationParameters deceleration)
expression - the expression whose evaluation will determine whether the until condition is met.deceleration - the rate of deceleration to stop at once the expression until condition is met.DistanceUntilNodeConfig createDistanceConfig()
Creates a Distance configuration for an Until node with PolyScope default values. This default configuration corresponds to when the end user inserts a new Until Distance node in the program tree manually.
Note that these default values may change between PolyScope versions.DistanceUntilNodeConfig createDistanceConfig(Length distance, ErrorHandler<Length> distanceErrorHandler, BlendParameters blendParameters)
distance - the distance for the robot arm to travel, not null.distanceErrorHandler - error handler for handling validation. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid distance value.blendParameters - the blend to be applied when the distance is met.ReachedWaypointUntilNodeConfig createReachedWaypointConfig()
IOInputUntilNodeConfig createIOInputConfig()
DigitalInputUntilNodeConfig createDigitalInputConfig(DigitalIO input, boolean valueToProceedUntil)
input - the digital input whose signal value will determine whether the until condition is met, not null.valueToProceedUntil - true, if the until condition is met when the input signal value goes HIGH,
false otherwise (condition met when signal value is LOW).IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().DigitalInputUntilNodeConfig createDigitalInputConfig(ModbusIO input, boolean valueToProceedUntil)
input - the digital MODBUS input whose value will determine whether the until condition is met, not null.valueToProceedUntil - true, if the until condition is met when the input signal value goes HIGH/true,
true otherwise (condition met when signal value is LOW).IllegalArgumentException - if input is an output (does not support reading of values)
or if output is not a digital output. See IO.isInput() and IO.getType().DigitalInputUntilNodeConfig createDigitalInputConfig(BooleanRegister input, boolean valueToProceedUntil)
true or false.input - the boolean input register whose value will determine whether the until condition is met, not null.valueToProceedUntil - true, if the until condition is met when the register value becomes true,
false otherwise (condition met when register value is false).IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().AnalogInputUntilNodeConfig createAnalogInputConfig(AnalogIO input, CompareOperator compareOperator, Current currentThreshold, ErrorHandler<Current> errorHandler)
input - the analog input whose signal value will determine whether the until condition is met, not null.compareOperator - the operator to use when comparing the signal value of the selected analog input to the
threshold value, not null. Available options are "less than" (<) or
"greater than" (>).currentThreshold - the electric Current threshold for the signal value of the analog input. Execution will
proceed until the signal value of the selected analog input goes past this threshold.errorHandler - the error handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid current value.IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().AnalogInputUntilNodeConfig createAnalogInputConfig(AnalogIO input, CompareOperator compareOperator, Voltage voltageThreshold, ErrorHandler<Voltage> errorHandler)
input - the analog input whose signal value will determine whether the until condition is met, not null.compareOperator - the operator to use when comparing the signal value of the selected analog input to the
threshold value, not null. Available options are "less than" (<) or
"greater than" (>).voltageThreshold - the electric Voltage threshold for the signal value of the analog input. Execution will
proceed until the signal value of the selected analog input goes past this threshold.errorHandler - the error handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid voltage value.IllegalArgumentException - if input is an output (does not support reading of values). See IO.isInput().FloatRegisterInputUntilNodeConfig createFloatRegisterInputConfig(FloatRegister input, CompareOperator compareOperator, float threshold)
input - the float input register whose value will determine whether the until condition is met, not null.compareOperator - the operator to use when comparing the value of the selected input register to the threshold
value, not null. Available options are "less than" (<) or "greater than"
(>).threshold - the threshold for the value of the float input register. Execution will proceed until the value
of the selected float input register goes past this threshold.IllegalArgumentException - if input is an output (does not support reading of values).
See IO.isInput().Copyright © 2021. All rights reserved.