public static enum PayloadNodeConfig.ConfigType extends Enum<PayloadNodeConfig.ConfigType>
Enum Constant and Description |
---|
CUSTOM_PARAMETERS
Custom payload parameters are specified.
|
PAYLOAD_SELECTION
A payload (from the installation) is selected.
|
Modifier and Type | Method and Description |
---|---|
static PayloadNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static PayloadNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final PayloadNodeConfig.ConfigType PAYLOAD_SELECTION
A payload (from the installation) is selected.
The config instance can be cast toSelectionPayloadNodeConfig
.public static final PayloadNodeConfig.ConfigType CUSTOM_PARAMETERS
Custom payload parameters are specified.
The config instance can be cast toCustomParametersPayloadNodeConfig
.public static PayloadNodeConfig.ConfigType[] values()
for (PayloadNodeConfig.ConfigType c : PayloadNodeConfig.ConfigType.values()) System.out.println(c);
public static PayloadNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2021. All rights reserved.