| Class and Description |
|---|
| MoveNodeConfig |
| MoveNodeConfigFactory
Deprecated.
Use the configuration builders available in
MoveNodeConfigBuilders interface which is accessible
through MoveNode.getConfigBuilders(). |
| TCPSelectionFactory
This interface supplies methods for creating TCP selections for a Move node configuration.
|
| Class and Description |
|---|
| FeatureSelection |
| FeatureSelection.SelectionType |
| MoveJMotionParameters |
| MoveJMoveNodeConfig |
| MoveLMotionParameters |
| MoveLMoveNodeConfig |
| MoveNodeConfig |
| MoveNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
| MoveNodeTCP |
| MovePMotionParameters |
| MovePMoveNodeConfig |
| TCPSelection |
| TCPSelection.SelectionType |
Copyright © 2021. All rights reserved.