public static enum TCPSelection.SelectionType extends Enum<TCPSelection.SelectionType>
Enum Constant and Description |
---|
IGNORE_ACTIVE_TCP
No TCP is used and the motion under this Move command will be with respect to the tool output flange.
|
TCP
A specific TCP is selected.
|
USE_ACTIVE_TCP
Motions are adjusted to the currently active TCP.
|
Modifier and Type | Method and Description |
---|---|
static TCPSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static TCPSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final TCPSelection.SelectionType USE_ACTIVE_TCP
public static final TCPSelection.SelectionType IGNORE_ACTIVE_TCP
public static final TCPSelection.SelectionType TCP
MoveNodeTCP
.public static TCPSelection.SelectionType[] values()
for (TCPSelection.SelectionType c : TCPSelection.SelectionType.values()) System.out.println(c);
public static TCPSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2021. All rights reserved.