public static enum LinearAxisSettings.LinearAxisSettingsType extends Enum<LinearAxisSettings.LinearAxisSettingsType>
Enum Constant and Description |
---|
COMPLIANT
The axis is compliant.
|
NON_COMPLIANT
The axis is non-compliant.
|
Modifier and Type | Method and Description |
---|---|
static LinearAxisSettings.LinearAxisSettingsType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static LinearAxisSettings.LinearAxisSettingsType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final LinearAxisSettings.LinearAxisSettingsType COMPLIANT
The axis is compliant.
This axis force setting instance can be cast toCompliantLinearAxisForce
.public static final LinearAxisSettings.LinearAxisSettingsType NON_COMPLIANT
The axis is non-compliant.
This axis limit setting instance can be cast toNonCompliantLinearAxisLimit
.public static LinearAxisSettings.LinearAxisSettingsType[] values()
for (LinearAxisSettings.LinearAxisSettingsType c : LinearAxisSettings.LinearAxisSettingsType.values()) System.out.println(c);
public static LinearAxisSettings.LinearAxisSettingsType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2021. All rights reserved.