public static enum DirectionMotionParameters.ParameterType extends Enum<DirectionMotionParameters.ParameterType>
Enum Constant and Description |
---|
SHARED_MOTION
The tool motion parameters are inherited from the MoveL or MoveP parent.
|
TOOL_MOTION
The tool motion parameters are selected.
|
Modifier and Type | Method and Description |
---|---|
static DirectionMotionParameters.ParameterType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static DirectionMotionParameters.ParameterType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final DirectionMotionParameters.ParameterType SHARED_MOTION
public static final DirectionMotionParameters.ParameterType TOOL_MOTION
ToolMotionParameters
.public static DirectionMotionParameters.ParameterType[] values()
for (DirectionMotionParameters.ParameterType c : DirectionMotionParameters.ParameterType.values()) System.out.println(c);
public static DirectionMotionParameters.ParameterType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2021. All rights reserved.