public interface ElseIfNode extends ProgramNode
| Modifier and Type | Method and Description |
|---|---|
String |
getExpression()
Deprecated.
Use
getExpression2() instead. |
Expression |
getExpression2() |
ElseIfNode |
setExpression(Expression expression) |
ElseIfNode |
setExpression(String expression)
Deprecated.
Use
ExpressionBuilder instead to build an Expression and set it using
setExpression(Expression expression). |
@Deprecated ElseIfNode setExpression(String expression)
ExpressionBuilder instead to build an Expression and set it using
setExpression(Expression expression).expression - The expression that will be evaluated in this ElseIfNode.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).ElseIfNode setExpression(Expression expression)
expression - The expression that will be evaluated in this ElseIfNode.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).@Deprecated String getExpression()
getExpression2() instead.Expression getExpression2()
Copyright © 2021. All rights reserved.