public interface SwingToolbarContribution
Defines an API required for specifying a PolyScope toolbar contribution. The contribution contains both the logic and UI of the toolbar.
Note: Toolbar contributions are not supported on CB3 robots.| Modifier and Type | Method and Description |
|---|---|
void |
buildUI(JPanel jPanel)
Build the UI for the toolbar on the provided panel.
|
void |
closeView()
Called each time the user exits this URCap toolbar in PolyScope.
|
void |
openView()
Called each time the user selects this URCap toolbar in PolyScope.
|
void buildUI(JPanel jPanel)
jPanel - the panel to build the UI on.void openView()
void closeView()
Copyright © 2021. All rights reserved.