public interface RegisteredCapabilities
Each of the individual grippers/zones available in a multi-gripper device supports all capabilities that has been
registered, i.e. all the individual grippers have the exact same set of capabilities. This interface gives access to
all registered capabilities, such as the width capability (see WidthCapability), speed capability (see
SpeedCapability), etc. This enables dynamic adjustment of capability properties, including the value range and
default values, exclusively per individual gripper (independently of the other grippers).
This interface is only relevant if the multi-gripper capability has been registered (using the method
GripperCapabilities.registerWidthCapability(double, double, double, double, Length.Unit)).
Each capability must be registered using the GripperCapabilities interface (when
GripperContribution.configureGripper(GripperConfiguration, GripperAPIProvider) is called) before they can be
accessed using this interface.
WidthCapability) returned when the capability was registered (with the GripperCapabilities interface).| Modifier and Type | Method and Description |
|---|---|
GripForceCapability |
getGripForceCapability()
Access the grip force capability interface which allows for dynamic adjustments of the capability properties
exclusively for this specific individual gripper (independently of the other grippers), including the value range
and default value.
|
GripVacuumCapability |
getGripVacuumCapability()
Access the grip vacuum capability interface which allows for dynamic adjustments of the capability properties
exclusively for this specific individual gripper (independently of the other grippers), including the value range
and default value.
|
SpeedCapability |
getSpeedCapability()
Access the speed capability interface which allows for dynamic adjustments of the capability properties exclusively
for this specific individual gripper (independently of the other grippers), including the value range and default
value.
|
WidthCapability |
getWidthCapability()
Access the width capability interface which allows for dynamic adjustments of the capability properties exclusively
for this specific individual gripper (independently of the other grippers), including the value range and default
value.
|
WidthCapability getWidthCapability()
Access the width capability interface which allows for dynamic adjustments of the capability properties exclusively for this specific individual gripper (independently of the other grippers), including the value range and default value.
This is only valid, if the width capability has been registered (using the methodGripperCapabilities.registerWidthCapability(double, double, double, double, Length.Unit)).UnsupportedOperationException - if the gripper has not registered the width capabilityGripForceCapability getGripForceCapability()
Access the grip force capability interface which allows for dynamic adjustments of the capability properties exclusively for this specific individual gripper (independently of the other grippers), including the value range and default value.
This is only valid, if the force capability has been registered (using the methodGripperCapabilities.registerGrippingForceCapability(double, double, double, Force.Unit)).UnsupportedOperationException - if the gripper has not registered the force capabilitySpeedCapability getSpeedCapability()
Access the speed capability interface which allows for dynamic adjustments of the capability properties exclusively for this specific individual gripper (independently of the other grippers), including the value range and default value.
This is only valid, if the speed capability has been registered (using the methodGripperCapabilities.registerSpeedCapability(double, double, double, double, Speed.Unit)).UnsupportedOperationException - if the gripper has not registered the speed capabilityGripVacuumCapability getGripVacuumCapability()
Access the grip vacuum capability interface which allows for dynamic adjustments of the capability properties exclusively for this specific individual gripper (independently of the other grippers), including the value range and default value.
This is only valid, if the vacuum capability has been registered (using the methodGripperCapabilities.registerGrippingVacuumCapability(double, double, double, Pressure.Unit)).UnsupportedOperationException - if the gripper has not registered the vacuum capabilityCopyright © 2021. All rights reserved.