public static enum Acceleration.Unit extends Enum<Acceleration.Unit>
| Enum Constant and Description |
|---|
IN_S2
Inches per second squared [in/s²] imperial unit.
|
M_S2
Meters per second squared [m/s²] SI unit.
|
MM_S2
Millimeters per second squared [mm/s²].
|
| Modifier and Type | Method and Description |
|---|---|
static Acceleration.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Acceleration.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Acceleration.Unit M_S2
public static final Acceleration.Unit MM_S2
public static final Acceleration.Unit IN_S2
public static Acceleration.Unit[] values()
for (Acceleration.Unit c : Acceleration.Unit.values()) System.out.println(c);
public static Acceleration.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2020. All rights reserved.