public interface ErrorHandler<V>
| Modifier and Type | Field and Description |
|---|---|
static ErrorHandler |
AUTO_CORRECT
Handler to automatically correct a value used for configuring a node when the value is not valid.
|
| Modifier and Type | Method and Description |
|---|---|
V |
onError(V invalidValue,
V nearestValidValue,
String errorMessage)
Callback in case of a validation error.
|
static final ErrorHandler AUTO_CORRECT
Handler to automatically correct a value used for configuring a node when the value is not valid.
Valid values depend on the constraints of the specific field. In most cases AUTO_CORRECT will use the nearest valid value.V onError(V invalidValue, V nearestValidValue, String errorMessage)
invalidValue - Value that violated a constraint.nearestValidValue - Acceptable value for field.errorMessage - Message describing the validation error.Copyright © 2020. All rights reserved.