public interface ToolIOInterface
| Modifier and Type | Interface and Description |
|---|---|
static class |
ToolIOInterface.OutputVoltage
Available options for the output voltage level for the power supply that delivers power to the connector in the
robot tool
|
| Modifier and Type | Method and Description |
|---|---|
AnalogInputModeConfig |
getAnalogInputModeConfig() |
DigitalOutputModeConfig |
getDigitalOutputModeConfig() |
ToolIOInterface.OutputVoltage |
getOutputVoltage() |
ToolIOInterface.OutputVoltage getOutputVoltage()
@RequiredCapability(value=DIGITAL_OUTPUT_MODE) DigitalOutputModeConfig getDigitalOutputModeConfig()
CapabilityNotSupportedException - if the digital output mode capability is not available on the system.
Use CapabilityManager.hasCapability(Capability) with ToolIOCapability.DIGITAL_OUTPUT_MODE to
verify the availability.AnalogInputModeConfig getAnalogInputModeConfig()
Copyright © 2020. All rights reserved.