public static enum CommunicationInterfaceConfig.BaudRate extends Enum<CommunicationInterfaceConfig.BaudRate>
| Enum Constant and Description |
|---|
BAUD_115200 |
BAUD_19200 |
BAUD_1M |
BAUD_2M |
BAUD_38400 |
BAUD_57600 |
BAUD_5M |
BAUD_9600 |
| Modifier and Type | Method and Description |
|---|---|
static CommunicationInterfaceConfig.BaudRate |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static CommunicationInterfaceConfig.BaudRate[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final CommunicationInterfaceConfig.BaudRate BAUD_9600
public static final CommunicationInterfaceConfig.BaudRate BAUD_19200
public static final CommunicationInterfaceConfig.BaudRate BAUD_38400
public static final CommunicationInterfaceConfig.BaudRate BAUD_57600
public static final CommunicationInterfaceConfig.BaudRate BAUD_115200
public static final CommunicationInterfaceConfig.BaudRate BAUD_1M
public static final CommunicationInterfaceConfig.BaudRate BAUD_2M
public static final CommunicationInterfaceConfig.BaudRate BAUD_5M
public static CommunicationInterfaceConfig.BaudRate[] values()
for (CommunicationInterfaceConfig.BaudRate c : CommunicationInterfaceConfig.BaudRate.values()) System.out.println(c);
public static CommunicationInterfaceConfig.BaudRate valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2020. All rights reserved.