public interface BlendParameters
| Modifier and Type | Interface and Description |
|---|---|
static class |
BlendParameters.ParameterType
Blend Parameters can be of different types
The parameter type is used to determine the explicit blend parameters (can be used in place of instanceof operations).
|
| Modifier and Type | Method and Description |
|---|---|
BlendParameters.ParameterType |
getType() |
BlendParameters.ParameterType getType()
Copyright © 2020. All rights reserved.