public static enum ExpressionOutputSelection.SelectionType extends Enum<ExpressionOutputSelection.SelectionType>
Enum Constant and Description |
---|
NO_OUTPUT
No output is selected.
|
OUTPUT
Output is selected.
|
UNRESOLVED_OUTPUT
The selected output is no longer available (e.g.
|
Modifier and Type | Method and Description |
---|---|
static ExpressionOutputSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static ExpressionOutputSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final ExpressionOutputSelection.SelectionType NO_OUTPUT
public static final ExpressionOutputSelection.SelectionType UNRESOLVED_OUTPUT
public static final ExpressionOutputSelection.SelectionType OUTPUT
Output is selected.
The Selection instance can be cast toExpressionOutput
.public static ExpressionOutputSelection.SelectionType[] values()
for (ExpressionOutputSelection.SelectionType c : ExpressionOutputSelection.SelectionType.values()) System.out.println(c);
public static ExpressionOutputSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.