public enum CompareOperator extends Enum<CompareOperator>
| Enum Constant and Description |
|---|
GREATER_THAN |
LESS_THAN |
| Modifier and Type | Method and Description |
|---|---|
static CompareOperator |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static CompareOperator[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final CompareOperator LESS_THAN
public static final CompareOperator GREATER_THAN
public static CompareOperator[] values()
for (CompareOperator c : CompareOperator.values()) System.out.println(c);
public static CompareOperator valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2020. All rights reserved.