IO.InterfaceType, IO.IOType| Modifier and Type | Method and Description |
|---|---|
String |
getIpAddress() |
String |
getSignalAddress() |
int |
getValue() |
boolean |
isResolvable()
A MODBUS I/O signal cannot be guaranteed to be present in PolyScope.
|
boolean |
setValue(int value) |
getDefaultName, getInterfaceType, getName, getType, getValueStr, isInputString getIpAddress()
String getSignalAddress()
boolean setValue(int value)
value - Set MODBUS signal to an integer value. If the MODBUS signal is digital, then false is
represented by 0 and true are represented by all numbers different from 0.true if the MODBUS signal was sent down to the controller, and false if the signal was
not sent down, e.g. because the controller was not running. Notice that the MODBUS signal must support writes,
consult the UR MODBUS protocol.int getValue()
false is represented by 0 and true is represented by the value 1.boolean isResolvable()
A MODBUS I/O signal cannot be guaranteed to be present in PolyScope. The end user can switch installation or delete the MODBUS signal. This method can be used to determine, if the MODBUS I/O is present.
NOTE: This method cannot be used to check connection status.isResolvable in interface IOtrue, if the MODBUS I/O is present in PolyScope.
false otherwise.Copyright © 2020. All rights reserved.