C - the (generic) type parameter for the interface representing the type of the ProgramNodeContribution
for which this view implements the UIpublic interface SwingProgramNodeView<C extends ProgramNodeContribution>
ProgramNodeContribution.
The instance of SwingProgramNodeView is a shared entity between several contributions.| Modifier and Type | Method and Description |
|---|---|
void |
buildUI(JPanel panel,
ContributionProvider<C> provider)
Build the UI for the corresponding
ProgramNodeContribution on the provided panel. |
void buildUI(JPanel panel, ContributionProvider<C> provider)
ProgramNodeContribution on the provided panel. Use the contribution
for your logic and data model manipulations.panel - the panel to build the UI onprovider - the provider for corresponding program node contribution currently selected (in the program tree)Copyright © 2020. All rights reserved.