public interface TouchEvent
Support for touch events from UI component.
NOTE: When also subscribing toInputEvent, the ordering of events is not guaranteed.| Modifier and Type | Interface and Description | 
|---|---|
static class  | 
TouchEvent.EventType
ON_PRESSED -  an event of this type is issued on mouse/touchscreen pressed. 
 | 
| Modifier and Type | Method and Description | 
|---|---|
HTMLComponent | 
getComponent()  | 
TouchEvent.EventType | 
getEventType()  | 
int | 
getRelativePosX()  | 
int | 
getRelativePosY()  | 
TouchEvent.EventType getEventType()
int getRelativePosX()
int getRelativePosY()
HTMLComponent getComponent()
Copyright © 2020. All rights reserved.