public interface InputCheckBox extends HTMLComponent
| Modifier and Type | Method and Description | 
|---|---|
String | 
getText()  | 
boolean | 
isSelected()  | 
void | 
setSelected(boolean selectedState)  | 
void | 
setText(String text)  | 
isEnabled, isVisible, setEnabled, setVisiblevoid setText(String text)
text - set the text associated with the input check box.String getText()
boolean isSelected()
true if the checkbox is checked, and false otherwise.void setSelected(boolean selectedState)
selectedState - make checkbox checked if true and unchecked otherwise.Copyright © 2020. All rights reserved.