public static enum Current.Unit extends Enum<Current.Unit>
| Enum Constant and Description | 
|---|
A
Ampere [A] SI unit. 
 | 
mA
Milliampere [mA]. 
 | 
| Modifier and Type | Method and Description | 
|---|---|
static Current.Unit | 
valueOf(String name)
Returns the enum constant of this type with the specified name. 
 | 
static Current.Unit[] | 
values()
Returns an array containing the constants of this enum type, in
the order they are declared. 
 | 
public static final Current.Unit A
public static final Current.Unit mA
public static Current.Unit[] values()
for (Current.Unit c : Current.Unit.values()) System.out.println(c);
public static Current.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2020. All rights reserved.