public interface Rotation
| Modifier and Type | Method and Description | 
|---|---|
boolean | 
epsilonEquals(Rotation other,
             double epsilon,
             Angle.Unit unit)
Indicates whether some other  
Rotation object is "approximately equal" to this one. | 
boolean | 
equals(Object obj)
Indicates whether some other  
Rotation object is "equal to" this one. | 
double | 
getRX()
Deprecated. 
 
Use  
getRX(Angle.Unit) instead. | 
double | 
getRX(Angle.Unit unit)
Provides the value of the Rx parameter in specified units. 
 | 
double | 
getRY()
Deprecated. 
 
Use  
getRY(Angle.Unit) instead. | 
double | 
getRY(Angle.Unit unit)
Provides the Ry parameter value in specified units. 
 | 
double | 
getRZ()
Deprecated. 
 
Use  
getRZ(Angle.Unit) instead. | 
double | 
getRZ(Angle.Unit unit)
Provides the Rz parameter value in specified units. 
 | 
int | 
hashCode()  | 
String | 
toString()  | 
@Deprecated double getRX()
getRX(Angle.Unit) instead.@Deprecated double getRY()
getRY(Angle.Unit) instead.@Deprecated double getRZ()
getRZ(Angle.Unit) instead.double getRX(Angle.Unit unit)
unit - the unit type.double value in specified units.double getRY(Angle.Unit unit)
unit - the unit type.double getRZ(Angle.Unit unit)
unit - the unit type.double value in specified units.boolean epsilonEquals(Rotation other, double epsilon, Angle.Unit unit)
Rotation object is "approximately equal" to this one.other - another Rotation object.epsilon - a tolerance.unit - the unit type of the epsilon tolerance.true if the value of this object is "approximately equal" to the value of the other
 argument; false otherwise.int hashCode()
boolean equals(Object obj)
Rotation object is "equal to" this one.Copyright © 2020. All rights reserved.