public interface PoseFactory
This interface provides methods for creating poses in Cartesian space (relative to a reference coordinate system).
A pose can, e.g. describe the position of the robot tool (e.g. w.r.t. to robot base) or the TCP offset (relative to the center of the tool output flange).| Modifier and Type | Method and Description | 
|---|---|
Pose | 
createPose(double x,
          double y,
          double z,
          double rx,
          double ry,
          double rz,
          Length.Unit lengthUnit,
          Angle.Unit angleUnit)
Creates a  
Pose object with the specified Cartesian position and orientation (rotation). | 
Pose createPose(double x, double y, double z, double rx, double ry, double rz, Length.Unit lengthUnit, Angle.Unit angleUnit)
Pose object with the specified Cartesian position and orientation (rotation).x - X coordinate of the position.y - Y coordinate of the position.z - Z coordinate of the position.rx - Rx parameter of the rotation vector specifying the orientation.ry - Ry parameter of the rotation vector specifying the orientation.rz - Rz parameter of the rotation vector specifying the orientation.lengthUnit - type of unit for the position.angleUnit - type of unit for the rotation.Copyright © 2020. All rights reserved.