T - the (generic) type parameter for the interface representing the type of input data being validated (e.g.
            Integer or Double).public interface InputValidator<T>
 Interface representing the input validators created by InputValidationFactory. This factory provides a set of
 standard input validators that can be used for validating the input entered by the user using the virtual keyboard/keypad.
 
InputValidationFactory does not satisfy your needs, you are free
 to implement your own custom validator.| Modifier and Type | Method and Description | 
|---|---|
String | 
getMessage(T value)
Returns a meaningful message in case the value is not valid. 
 | 
boolean | 
isValid(T value)  | 
boolean isValid(T value)
value - to be validated.true if value is valid.Copyright © 2020. All rights reserved.