@ProviderType
public interface TreeNode
This interface represents a node in the program tree that can be used to construct a sub-tree rooted in a URCap program node.
Using theProgramModel.getRootTreeNode(ProgramNodeContribution) to obtain a root for the sub-tree, it is
possible to add children. For each call to addChild(ProgramNode), a new TreeNode is returned,
that can, in turn, act as a root for yet another sub-tree.| Modifier and Type | Method and Description |
|---|---|
TreeNode |
addChild(ProgramNode programNode)
Add a child program node to the sub-tree.
|
List<TreeNode> |
getChildren() |
ProgramNode |
getProgramNode() |
TreeNode |
insertChildAfter(TreeNode existingChildNode,
ProgramNode programNode)
Inserts a child program node under in the sub-tree directly after the existing selected child node.
|
TreeNode |
insertChildBefore(TreeNode existingChildNode,
ProgramNode programNode)
Inserts a child program node in the sub-tree directly before the existing selected child node.
|
TreeNode |
locateDescendantTreeNode(ProgramNode programNode)
Gets a corresponding
TreeNode instance for a child program node (a ProgramNode instance) in the
sub-tree under this TreeNode. |
boolean |
removeChild(TreeNode child)
Removes a child node from the sub-tree.
|
TreeNode |
setChildSequenceLocked(boolean isChildSequenceLocked)
Configures whether or not child nodes can be rearranged, deleted or have other nodes inserted into the child
sequence by the end user.
|
void |
traverse(ProgramNodeVisitor nodeVisitor)
This method traverses the entire sub-tree under this tree node in a depth-first fashion (this corresponds to a
top-down approach in the program tree).
|
TreeNode addChild(ProgramNode programNode) throws TreeStructureException
programNode - the ProgramNode constructed using the ProgramNodeFactoryTreeStructureException - If it is not allowed to insert the ProgramNode at this position a
TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).TreeNode insertChildBefore(TreeNode existingChildNode, ProgramNode programNode) throws TreeStructureException
existingChildNode - existing TreeNode child of this TreeNode.programNode - the ProgramNode constructed using the ProgramNodeFactory.TreeStructureException - If it is not allowed to insert the ProgramNode at this position or if the
selected child node is not a child of this TreeNode a TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).TreeNode insertChildAfter(TreeNode existingChildNode, ProgramNode programNode) throws TreeStructureException
existingChildNode - existing TreeNode child of this TreeNode.programNode - the ProgramNode constructed using the ProgramNodeFactory.TreeStructureException - If it is not allowed to insert the ProgramNode at this position or if the
selected child node is not a child of this TreeNode a TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).boolean removeChild(TreeNode child) throws TreeStructureException
child - The TreeNode child to be removed.true if removed successfully. false otherwise.TreeStructureException - If the removed child would leave the tree in an illegal state a
TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).List<TreeNode> getChildren()
TreeNode objects that represents all the children of this TreeNode (both
programmatically added as well as inserted by the end user).ProgramNode getProgramNode()
ProgramNode at this position in the sub-tree.
Can either be a built-in PolyScope program node (provided by Universal Robots) or a URCap program node.TreeNode locateDescendantTreeNode(ProgramNode programNode)
Gets a corresponding TreeNode instance for a child program node (a ProgramNode instance) in the
sub-tree under this TreeNode.
ProgramNodeVisitor (or any derived sub class thereof).programNode - program node to get a corresponding TreeNode representation for, not null.
Can either be a built-in PolyScope program node (provided by Universal Robots) or a URCap
program node.TreeNode instance for the specified program node.ProgramNodeNotInSubTreeException - when the program node cannot be found because it is not in the sub-tree.TreeNode setChildSequenceLocked(boolean isChildSequenceLocked)
isChildSequenceLocked - If true then the immediate children under this TreeNode will be locked.void traverse(ProgramNodeVisitor nodeVisitor)
This method traverses the entire sub-tree under this tree node in a depth-first fashion (this corresponds to a top-down approach in the program tree).
A node visitor is used for callbacks to the visit-overloads you choose to override. The overload called depends on the node type encountered. Override the overloads for the node types you are concerned with. All visit-methods have the program node, sibling index and depth as arguments to help filter nodes if needed.
The node visitor can be either a ProgramNodeVisitor implementation with optional overrides or a
URCapProgramNodeInterfaceVisitor implementation. In the latter case, the
URCapProgramNodeInterfaceVisitor.visitURCapAs(Object, int, int) method must be implemented.
The URCapProgramNodeInterfaceVisitor can be used when targeting URCap program nodes implementing the
(generic) type parameter specified in URCapProgramNodeInterfaceVisitor (see also
URCapProgramNode.getAs(Class)).
accept() in the Visitor software design pattern.nodeVisitor - the instance callbacks are made to.Copyright © 2020. All rights reserved.