public static enum FixedPositionWaypointNodeConfig.PositionDefinition extends Enum<FixedPositionWaypointNodeConfig.PositionDefinition>
| Enum Constant and Description | 
|---|
DEFINED
 The position of the waypoint has been defined. 
 | 
UNDEFINED
The position has not been defined. 
 | 
| Modifier and Type | Method and Description | 
|---|---|
static FixedPositionWaypointNodeConfig.PositionDefinition | 
valueOf(String name)
Returns the enum constant of this type with the specified name. 
 | 
static FixedPositionWaypointNodeConfig.PositionDefinition[] | 
values()
Returns an array containing the constants of this enum type, in
the order they are declared. 
 | 
public static final FixedPositionWaypointNodeConfig.PositionDefinition UNDEFINED
public static final FixedPositionWaypointNodeConfig.PositionDefinition DEFINED
The position of the waypoint has been defined.
Cast this instance toFixedPositionDefinedWaypointNodeConfig.public static FixedPositionWaypointNodeConfig.PositionDefinition[] values()
for (FixedPositionWaypointNodeConfig.PositionDefinition c : FixedPositionWaypointNodeConfig.PositionDefinition.values()) System.out.println(c);
public static FixedPositionWaypointNodeConfig.PositionDefinition valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2020. All rights reserved.