public static enum WaitNodeConfig.ConfigType extends Enum<WaitNodeConfig.ConfigType>
Enum Constant and Description |
---|
ANALOG_INPUT_CURRENT
Analog input configured for electric current or no input has been selected.
|
ANALOG_INPUT_VOLTAGE
Analog input configured for voltage has been selected.
|
DIGITAL_INPUT
Digital input has been selected.
|
EXPRESSION_INPUT
Expression has been selected.
|
FLOAT_REGISTER_INPUT
Input register using float type values has been selected.
|
NO_TYPE
No selection has been made.
|
NO_WAIT
No wait has been selected.
|
TIME
Time to wait has been selected.
|
Modifier and Type | Method and Description |
---|---|
static WaitNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static WaitNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final WaitNodeConfig.ConfigType NO_TYPE
public static final WaitNodeConfig.ConfigType NO_WAIT
public static final WaitNodeConfig.ConfigType TIME
Time to wait has been selected.
The config instance can be cast toTimeWaitNodeConfig
.public static final WaitNodeConfig.ConfigType DIGITAL_INPUT
Digital input has been selected.
The config instance can be cast toDigitalInputWaitNodeConfig
.public static final WaitNodeConfig.ConfigType ANALOG_INPUT_CURRENT
Analog input configured for electric current or no input has been selected.
The config instance can be cast toAnalogInputCurrentWaitNodeConfig
.public static final WaitNodeConfig.ConfigType ANALOG_INPUT_VOLTAGE
Analog input configured for voltage has been selected.
The config instance can be cast toAnalogInputVoltageWaitNodeConfig
.public static final WaitNodeConfig.ConfigType FLOAT_REGISTER_INPUT
Input register using float type values has been selected.
The config instance can be cast toFloatRegisterInputWaitNodeConfig
.public static final WaitNodeConfig.ConfigType EXPRESSION_INPUT
Expression has been selected.
The config instance can be cast toExpressionInputWaitNodeConfig
public static WaitNodeConfig.ConfigType[] values()
for (WaitNodeConfig.ConfigType c : WaitNodeConfig.ConfigType.values()) System.out.println(c);
public static WaitNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.