public static enum FloatRegisterInputSelection.SelectionType extends Enum<FloatRegisterInputSelection.SelectionType>
Enum Constant and Description |
---|
FLOAT_REGISTER_INPUT
Float register input is selected.
|
NO_FLOAT_REGISTER_INPUT
No float register input is selected.
|
Modifier and Type | Method and Description |
---|---|
static FloatRegisterInputSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static FloatRegisterInputSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final FloatRegisterInputSelection.SelectionType NO_FLOAT_REGISTER_INPUT
public static final FloatRegisterInputSelection.SelectionType FLOAT_REGISTER_INPUT
Float register input is selected.
The Selection instance can be cast toFloatRegisterInput
.public static FloatRegisterInputSelection.SelectionType[] values()
for (FloatRegisterInputSelection.SelectionType c : FloatRegisterInputSelection.SelectionType.values()) System.out.println(c);
public static FloatRegisterInputSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.