public static enum AnalogInputSelection.SelectionType extends Enum<AnalogInputSelection.SelectionType>
Enum Constant and Description |
---|
ANALOG_INPUT
Analog input is selected.
|
NO_ANALOG_INPUT
No analog input is selected.
|
Modifier and Type | Method and Description |
---|---|
static AnalogInputSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AnalogInputSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final AnalogInputSelection.SelectionType NO_ANALOG_INPUT
public static final AnalogInputSelection.SelectionType ANALOG_INPUT
Analog input is selected.
The Selection instance can be cast toAnalogInput
.public static AnalogInputSelection.SelectionType[] values()
for (AnalogInputSelection.SelectionType c : AnalogInputSelection.SelectionType.values()) System.out.println(c);
public static AnalogInputSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.