public static enum FloatRegisterOutputSelection.SelectionType extends Enum<FloatRegisterOutputSelection.SelectionType>
Enum Constant and Description |
---|
FLOAT_REGISTER_OUTPUT
Float register output is selected.
|
NO_FLOAT_REGISTER_OUTPUT
No float register output is selected
|
Modifier and Type | Method and Description |
---|---|
static FloatRegisterOutputSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static FloatRegisterOutputSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final FloatRegisterOutputSelection.SelectionType NO_FLOAT_REGISTER_OUTPUT
public static final FloatRegisterOutputSelection.SelectionType FLOAT_REGISTER_OUTPUT
Float register output is selected.
The Selection instance can be cast toFloatRegisterOutput
.public static FloatRegisterOutputSelection.SelectionType[] values()
for (FloatRegisterOutputSelection.SelectionType c : FloatRegisterOutputSelection.SelectionType.values()) System.out.println(c);
public static FloatRegisterOutputSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.