public static enum LoopNodeConfig.ConfigType extends Enum<LoopNodeConfig.ConfigType>
Enum Constant and Description |
---|
ALWAYS
Looping infinitely has been selected.
|
COUNTER
Looping a certain number of times has been selected.
|
EXPRESSION
Looping as long as the evaluation of an expression is true has been selected.
|
Modifier and Type | Method and Description |
---|---|
static LoopNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static LoopNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final LoopNodeConfig.ConfigType ALWAYS
Looping infinitely has been selected.
The config instance can be cast toAlwaysLoopNodeConfig
public static final LoopNodeConfig.ConfigType COUNTER
Looping a certain number of times has been selected.
The config instance can be cast toCounterLoopNodeConfig
public static final LoopNodeConfig.ConfigType EXPRESSION
Looping as long as the evaluation of an expression is true has been selected.
The config instance can be cast toExpressionLoopNodeConfig
public static LoopNodeConfig.ConfigType[] values()
for (LoopNodeConfig.ConfigType c : LoopNodeConfig.ConfigType.values()) System.out.println(c);
public static LoopNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.