public interface WaypointNode extends ProgramNode
| Modifier and Type | Method and Description |
|---|---|
WaypointNodeConfig |
getConfig() |
WaypointNodeConfigFactory |
getConfigFactory() |
WaypointNode |
setConfig(WaypointNodeConfig config)
Set a configuration on this node.
|
WaypointNodeConfigFactory getConfigFactory()
WaypointNode setConfig(WaypointNodeConfig config)
config - the configuration to be set.IllegalArgumentException - If the configuration does not match the Move node type.
e.g. trying to apply JointMotionParameters to a MoveL.IllegalArgumentException - if inverse kinematics cannot find corresponding joint position to this pose including TCPIllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).WaypointNodeConfig getConfig()
Copyright © 2020. All rights reserved.