C - the (generic) type parameter for the interface representing the type of the
             InstallationNodeContribution for which this view implements the UIpublic interface SwingInstallationNodeView<C extends InstallationNodeContribution>
InstallationNodeContribution| Modifier and Type | Method and Description | 
|---|---|
void | 
buildUI(JPanel panel,
       C contribution)
Build the UI for the corresponding  
InstallationNodeContribution on the provided panel. | 
void buildUI(JPanel panel, C contribution)
InstallationNodeContribution on the provided panel. Use the contribution
 for your logic and data model manipulations.panel - the panel to build the UI oncontribution - the corresponding installation node contribution.Copyright © 2020. All rights reserved.