public static enum CreationContext.NodeCreationType extends Enum<CreationContext.NodeCreationType>
Enum Constant and Description |
---|
LOAD
This node was created as the result of loading an installation
|
NEW
This node was created as the result of creating a new installation.
|
Modifier and Type | Method and Description |
---|---|
static CreationContext.NodeCreationType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static CreationContext.NodeCreationType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final CreationContext.NodeCreationType NEW
public static final CreationContext.NodeCreationType LOAD
public static CreationContext.NodeCreationType[] values()
for (CreationContext.NodeCreationType c : CreationContext.NodeCreationType.values()) System.out.println(c);
public static CreationContext.NodeCreationType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.