public interface SystemConfiguration
| Modifier and Type | Method and Description | 
|---|---|
CapabilityManager | 
getCapabilityManager()
Access an interface that can be used for verifying that specific capabilities are available on the underlying
 robot/system. 
 | 
ControllableResourceModel | 
getControllableResourceModel()
 Access an interface for requesting exclusive control of system resources, e.g. 
 | 
ResourceModel | 
getResourceModel()  | 
CapabilityManager getCapabilityManager()
RequiredCapability.ResourceModel getResourceModel()
ControllableResourceModel getControllableResourceModel()
Access an interface for requesting exclusive control of system resources, e.g. the configuration of the Tool I/O Interface.
NOTE: Requesting control of a system resource must happen in the scope of theScrewdriverContribution.configureInstallation(CustomUserInputConfiguration, SystemConfiguration, TCPConfiguration, ScrewdriverAPIProvider)
 method.Copyright © 2020. All rights reserved.