public interface ContributionConfiguration
| Modifier and Type | Method and Description | 
|---|---|
void | 
setLogo(Icon logo)
Provide a custom logo that will be displayed in PolyScope in:
 
   The builtin (native) PolyScope Screwdriving installation screen at the top where the screwdriver
       is selected.
   The screen for the builtin (native) PolyScope Screwdriving program node (if this screwdriver
       has been selected in the Screwdriving installation screen)
  
 | 
void setLogo(Icon logo)
The provided logo will be scaled automatically, if necessary.
If no custom logo is provided, a default logo will be displayed instead.logo - The logo to be shown in PolyScopeCopyright © 2020. All rights reserved.