T
- The (generic) type parameter for the interface representing the type of input data entered or selected by
the end user. Relevant types are, e.g. Integer
and Double
.public interface ValueChangedListener<T>
This interface can be used to listen for changes of the value of a user input.
Implement this interface to execute custom code when the end user has entered or selected a new value as well as when a new installation is loaded or created.Modifier and Type | Method and Description |
---|---|
void |
onValueChanged(T value)
Called upon a change of the current value of the user input.
|
void onValueChanged(T value)
value
- The new value.Copyright © 2020. All rights reserved.