public interface TextComponent
| Modifier and Type | Method and Description | 
|---|---|
void | 
setIcon(Icon icon)
 Updates the icon to be displayed to the end user. 
 | 
void | 
setText(String text)
Updates the text to be displayed to the end user. 
 | 
void setIcon(Icon icon)
Updates the icon to be displayed to the end user.
Supports 24x24 pixels icons for CB3 robots and 30x30 pixel icons for e-Series robots. The provided icon will be scaled automatically, if necessary.icon - The icon to be displayed. Passing null is allowed and will clear the icon.void setText(String text)
text - The text to be displayed, not null.Copyright © 2020. All rights reserved.