public abstract class RobotPositionCallback extends Object
| Constructor and Description |
|---|
RobotPositionCallback() |
| Modifier and Type | Method and Description |
|---|---|
void |
onCancel()
This method is called if the end user cancels inputting the robot position.
|
abstract void |
onOk(Pose pose,
JointPositions q)
This method is called if the end user accepts the robot position.
|
public abstract void onOk(Pose pose, JointPositions q)
pose - the pose of the robot.q - the joint positions of the robot.public void onCancel()
Copyright © 2019. All rights reserved.