| Enum | Description | 
|---|---|
| BlendParameters.ParameterType | The blend parameters type used to determine which type of blend parameters this instance is. | 
| FixedPositionWaypointNodeConfig.PositionDefinition | |
| VariablePositionWaypointNodeConfig.VariableDefinition | |
| WaypointMotionParameters.ParameterType | |
| WaypointNodeConfig.ConfigType | The configuration type used to determine which type of configuration this instance is. | 
Copyright © 2019. All rights reserved.